DUG_ITRV_LK-01

Using the device

When a Thermostat is commissioned and assigned to a room, a group is automatically created with all the Thermostats from the same room. This group is called as Radiator Thermostats in the home page. This grouping is to save heating costs and to avoid Thermostats working against each other in a room.

NOTE: The individual Thermostats will not appear on the home page by default. To change this setting, refer to Individual Thermostat visibility on home page.

Group Thermostat control panel

On the group Thermostat control panel page, you can see the following:
  • The current temperature value (A)

  • The setpoint temperature value (B)

  • The sliding bar to adjust the temperature (C)

  • Boost mode (D)

  • History (E)

  • Schedule (F)


Individual Thermostat control panel

On the individual Thermostat control panel page, you can see the following:
NOTE: This control panel will not have the slider bar as you cannot control the temperature of the Thermostats individually. To adjust the setpoint, check the Group Thermostat control panel.
  • Battery (A)

  • The current temperature value (B)

  • The setpoint temperature value (C)

  • History (D)

  • Settings (E)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?