DUG_Exxact - ZB Thermostat 16 A_WSE-00

Setting the room temperature manually

The room temperature can be increased/decreased manually by pressing the touch button of the thermostat.
  • Press the “+” button to increase the temperature setpoint.

  • Press the “” button to decrease the temperature setpoint.

In P3, P5, P6, if floor sensor is fitted, device will be in room temperature with floor limits mode.

When the room temperature is at or above the current setpoint, the floor temperature is below the lower floor temperature limit (min. guard), the demand is generated and the room is heated to warm the floor, and the demand LED flashes white at 1 Hz.

When the room temperature is below the current setpoint, the floor temperature is above the upper floor temperature limit (max. guard), the demand should be 0 and control output should be prevented, the demand LED flashes white at 1 Hz.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?