DUG_Exxact - ZB Thermostat 16 A_WSE-00

Enabling individual thermostat visibility on home page

The individual thermostats will not appear on the home page by default. Using the app, you can change the default settings to adjust the visibility according to your preferences.
  1. On the Home page, tap All devices > Thermostat.
  2. Tap to display more details.
  3. Tap thetoggle switch (A) to enable or disable the Show Individual CFMT in Home Page option.
    NOTE:
    • By enabling, individual thermostat is shown in the home page and disabling it hides the individual thermostat in home page.

    • Tapping for more menu in the individual thermostat control panel, allows you to update firmware and remove the device from the system.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?