DUG_Exxact - ZB Thermostat 16 A_WSE-00

Schedule actions within boost period

When boost mode is enabled during this period, the system will temporarily stop the scheduled actions and only perform the boost operation until the boost duration is over.

The new action always has a higher priority than the current action. As a result, boost mode will be activated even when the scheduled action is in progress and the system will stop the schedule.

To view the temperature changes during the boost operation, go to Checking the device history.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?