Setting boost mode manually
When enabled the temperature increases by 2° C for temperature control modes (P1 to P8) and by +2 for regulator mode (P9) over the setpoint.
To enable boost mode:
-
Press O button once to enter boost menu.
+1 flashes on thermostat matrix. -
Use +/- button to navigate between the boost hours from +1 to +3.
After selecting the boost hours, thermostat will save and exit boost mode if there is no interaction within 5 s.
For example:
If current setpoint is 12° C and
you enable boost mode by selecting +3.
The boost mode
will set the setpoint temperature to 14° C for next 3 hours.
After 3 hours setpoint will return to 12° C.
To disable boost mode:
-
Press O button once.
+1 flashes on thermostat matrix. -
Press + button for thermostat to display – – (boost cancel).
After selecting the boost cancel, thermostat will save and exit boost mode if there is no interaction within 5 s.