DUG_Exxact - ZB Thermostat 16 A_WSE-00

Creating a moment

A Moment allows you to group multiple actions that are usually done together. Using the Wiser app, you can create moments based on your needs.
  1. On the Home page, tap .
  2. Go to Moment > + to create a moment.
  3. Tap Edit name to enter the name of moment (A) and tap Save.
    TIP: You can choose the cover image that represents your moment by tapping .
  4. In the Action section, tap Add task (B) to open the slide-up menu.
  5. In the Add task menu, you can do either or all of the following actions (C):
    • Run the device - Select the devices that you want in a moment
    • Select Automation - Select the automation that you want to enable or disable
    • Delay - Set the delay time
    NOTE: You can add one or more actions using .
  6. Tap Run the device > Thermostat to select one or more functions to add in the moment:
    • Temperature Setpoint: Increase the thermostat's temperature according to your requirement (D).
    • Heating Boost: Increase the temperature by setting the boost duration (E).
  7. Once all the actions are set, tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?