DUG_Exxact - ZB Thermostat 16 A_WSE-00

Manual sensor settings

A thermostat with a preset value of P6 to P8 can be connected with an external floor sensor to increase the user's experience in regulating the temperature.
NOTE: Once the preset is chosen, press O button for 1 second to confirm. Then the device continues to the sensor setting in the below sequence. For more info on preset, refer device presetting

Selecting floor sensor type

After preset, you will enter floor sensor selection menu where you can manually select the sensor type connected to the thermostat after setting the preset; this allows the thermostat to convert and display the temperature accurately.

To select the floor sensor type:

  1. Once you enter the selection menu, “10” will be displayed on the thermostat dot matrix. Press + or touch button on the device to switch between the sensor types.
    Following are the available sensor type:

    • 10 kOhm

    • 12 kOhm

    • 15 kOhm

    • 33 kOhm

    • 47 kOhm


    TIP: When + button is pressed, sensor type 10 becomes 12, continue to press the + button, and the type changes to 15, 33, and 47.
    When button is pressed, sensor type 47 becomes 33, continue to press the button, and the type changes to 15, 12, and 10.

  2. Select the sensor type which is installed and then press the O touch button for > 1 s to confirm the selection.

The thermostat dot-matrix display the sensor type and LED flashes blue.

Setting temperature calibration

After selecting the floor sensor type, you must set the calibration value (offset value) of the sensor in order to minimize any variation in temperature measurement.

To set temperature calibration:

  1. Press + or touch button on the device to set the calibration value between.

    NOTE: The temperature calibration ranges from -9°C to +9°C and can be adjusted in 0.5°C increments.
  2. Set the calibration value, press the O touch button for > 1 s to confirm the selection.

The thermostat dot-matrix display calibration value and LED flashes purple.

Setting maximum guard temperature

After setting temperature calibration, you must set the maximum guard temperature. It is upper limit of the floor sensor.
Minimum guard temperature can only be set through Wiser app.

To set maximum guard temperature:

  1. Press + or touch button on the device to set the maximum limit.

    NOTE: The temperature limit ranges from 11°C to 40°C.
  2. Set the value, press the O touch button for > 1 s to confirm the selection.

The thermostat dot-matrix display calibration value and LED flashes red.

IMPORTANT:
  • If you want to update the sensor settings manually after setting up the device, Press O and + button simultaneously to enter preset selection and press O to confirm preset and enter sensor setting.

  • You can also perform a factory reset to remove all settings and configure the thermostat newly. Refer resetting the device.

  • It is possible to modify or update sensor settings without resetting the thermostat with the Wiser app. Refer app settings

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?