Pairing device manually
- On the Home page, tap +.
- Tap
and select the required Wiser HUB on the slide-up menu.
- Select an option to add the device (A):
- Add Device with Install Code
- Add Device without Install Code
- To pair the device with an install code, tap Add Device with Install Code to display the slide-up
menu. Select any one of the options (B):
- Scan Install Code - you can scan the device for the install code.
- Enter Install Code Manually - you can manually enter the install code from the device.
After pairing the device with install code, proceed to Step 6. - To pair the device without install code, tap Add Device without Install Code.
- Long press the O button until Jn is displayed
and then release the button to initiate joining.NOTE: If you have already paired your thermostat, and want to change the preset mode during the current pairing process, you will need to perform a factory reset. Otherwise, the thermostat will be paired with the previous preset mode. Refer resetting the device.
- In the app, tap Confirm device display Jn and than tap Start Configuration (C).
- Wait for a few seconds until the wireless
LED on the thermostat turns green.
- After the device is added in the app, assign a room to
enable settings and than tap Done.NOTE:
-
Assigning a room, creates a group to control the thermostats, refer using the device.
-
Refer changing the device location to assign a room to the thermostat, if you did not assign the room at Step 9.
-