Screen brightness settings
Active brightness level
You can configure the brightness of the LEDs when the thermostat is active (during interaction):
-
Tap Active Brightness Level (A).
-
On the slide up menu, adjust the desired brightness level then tap Save.
-
Default active screen brightness is 100%
-
The screen brightness range is 1%~100%, and the setting accuracy is 1%.
Idle brightness level
You can configure the brightness of the LEDs when thermostat is inactive (after time-out of screen active brightness).
-
Tap Idle Brightness Level (B).
-
On the slide up menu, adjust the desired brightness level then tap Save.
-
Default idle screen brightness is 0%
-
The screen brightness range is 0%~100% and it should not be more than active brightness level.
Screen active duration
The thermostat can be configured to set a timeout for the LED when it is active.
-
Tap Screen Active Duration (C).
-
On the slide up menu, select required active duration:
-
5 Secs
-
10 Secs
-
30 Secs
-
45 Secs
-
Customized Duration: use +/- or drag the sliding bar to change the Active Duration, which ranges from 1 minute to 60 minutes.
NOTE: Default screen active duration is 60 s.
-