DUG_Exxact - ZB Thermostat 16 A_WSE-00

Managing device settings using Wiser app

Using the Wiser app, you can manage the thermostat settings.

To access the settings:

  1. On the Home page, tap All devices > Thermostat.

  2. On the device control panel page, tap Settings.

All setting option in the Wiser app is based on the preset value set during paring process.

Preset Valve
protection
Air
calibration
setting
Sensor
type
selection
Floor
calibration
setting
Max/Min
guard
temp.
setting
Child
lock
Rated
power
value
Screen
brightness
settings
P1 ü ü x x x ü x ü
P2 ü ü x x x ü x ü
P3 ü ü ü ü ü ü x ü
P4 x ü x x x ü ü ü
P5 x ü ü ü ü ü ü ü
P6 x ü ü ü ü ü ü ü
P7 ü x ü ü ü ü x ü
P8 x x ü ü ü ü ü ü
P9 x x x x x ü ü ü

Valve protection

Air calibration setting

Sensor type selection

Floor calibration setting

Max/Min guard temp. setting

Child lock

Rated power value

Screen brightness settings

Below are the setting interface based on preset:

P1 and P2 P3 P4
P5 and P6 P7
P8 P9

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?