Pairing device with auto scan
- On the Home page, tap +.
- Tap .
- Enable permissions to Access location and Wi-Fi for scanning device and tap Start scanning.NOTE: If you have multiple hubs, do Step 4 or proceed to Step 5.
- Tap Select hub and select the Wiser HUB from the slide-up menu.
- Long press the O button until 'Jn' is displayed
and then release the button to initiate joining.NOTE: If you have already paired your thermostat, and want to change the preset mode during the current pairing process, you will need to perform a factory reset. Otherwise, the thermostat will be paired with the previous preset mode. Refer resetting the device.TIP: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds.
- Wait for a few seconds until the device search is complete, than tap Next (A) and select Thermostat 16 A.
- Once the device is paired successfully, assign a room to
enable settings and than tap Done.NOTE:
-
Assigning a room, creates a group to control the thermostats, refer using the device.
-
Refer changing the device location to assign a room to the thermostat, if you did not assign the room at Step 7.
-