SUG_Wiser_Sweden_Finland_WSE-09

OTA

(Over the air) Refers to the method of updating the firmware in a device. Example: Perform an OTA update of firmware on a device using the app.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.