SUG_Wiser_Sweden_Finland_WSE-09

Switching the gateway Ethernet connection to Wi-Fi (optional)

Use Wi-Fi to connect the gateway to the network router so that the Ethernet cable is no longer needed.

Before doing this task, confirm that the mobile phone/tablet and gateway are both connected to the Wi-Fi network router.

  1. In the app, select the gateway to the same Wi-Fi network.
    NOTE: At this stage, the Ethernet cable should be still connected.
  2. Tap the Settings (gear) icon (A).

  3. In the Settings page, tap IP Network Setting(B).

  4. Tap the Wi-Fi tab, set the SSID and Password for the Wi-Fi network router and then tap Apply(C).

  5. Once the Wi-Fi connection is successful, remove the Ethernet cable from the gateway.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.