SUG_Wiser_Sweden_Finland_WSE-09

Heat device

Wiser Radiator Thermostat

The Wiser Radiator Thermostat uses integrated temperature sensors to control the flow of water through a radiator, thereby regulating the temperature in a room. The target temperature and switching times are set in the Wiser App.

Instruction Sheet (PDF)

Device User Guide

Exxact - Connected Thermostat Room/Floor 16 A

The Connected Thermostat Room/Floor 16 A is mainly used for electric underfloor heating or electric radiators, but could also be used to control mains powered motorized valves or circulating pumps for water-based heating.

Instruction Sheet (PDF)

Device User Guide

Renova - Connected Thermostat Room/Floor 16 A

The Connected Thermostat Room/Floor 16 A is mainly used for electric underfloor heating or electric radiators, but could also be used to control mains powered motorized valves or circulating pumps for water-based heating

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.