SUG_Wiser_Sweden_Finland_WSE-09

Checking for any device requiring a firmware upgrade

  1. On the Home page, tap the Menu icon (A) .
  2. In the menu slide-out, tap Firmware Upgrade(B) .
  3. Tap a device in the Devices to be updated list(C) and follow the instructions in the app.
  4. Tap the button beside Automatically updated(D) to enable automatic updates.
    After this, a notification is received that the firmware is updated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.