SUG_Wiser_Sweden_Finland_WSE-09

Energy device

PowerTag Energy

PowerTag is a compact, robust, and easy-to-install wireless communication energy sensor. It is used together with the Gateway/Hub to collect information from every equipped circuit to identify the energy consumption of each connected load. It is designed specifically to manage energy consumption for new and existing residential installations. It monitors and measures energy and power in real-time, and also provides complete visibility of power transfer between power source and loads.

Instruction Sheet-F63 (PDF)

Instruction Sheet-M63 (PDF)

Device User Guide

EVlink Home Smart

EVlink Home Smart provides homeowners with an easy and smart charging experience. The Wiser app for residential energy management enables easy access to monitor and control their charging experience remotely.

Installation Instructions

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.