SUG_Wiser_Sweden_Finland_WSE-09

Device button/key and LED locations

Find the location of buttons, keys and LED indicators on various devices.

Wiser Micro Module Light Switch/Shades Control

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

(See A) Setup/Reset button. Press 3 times on the rocker to activate.

(See B) Status LED

Wiser Micro Module Dimmer

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

(See A) Setup/Reset button. Press 3 times on the rocker to activate.

(See B) Status LED

Wiser Relay Switch 10 A/Universal Push-Button Dimmer LED/Blind Control Switch/Connected Multiwire Universal Push-button Dimmer LED

(See A) Push button

(See B) Status LED

Wiser Motion Sensor with Switch 10 A/with Universal Push-button Dimmer LED

(See A) Push button

(See B) Status LED

Wiser Universal Rotary Dimmer LED/Connected Multiwire Universal Rotary Dimmer LED

(See A) Rotary button shaft

(See B) Status LED

Wiser Window/Door Sensor

(See A) Function key

(See B) Status LED (visible on front of master part when flashing or lit)

Wiser Motion Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser Water Leakage Sensor

(See A) Function key

(See B) Status LED (visible on top of sensor when flashing or lit)

Wiser Temperature/Humidity Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser SmartPlug 16 A

(See A) Operation button

(See B) Status LED

Wiser IP Camera Indoor

(See A) Micro SD Card slot

(See B) Status LED

(See C) Reset Button

IP Camera Outdoor

(See A) Reset button

(See B) Micro SD Card slot

(See C) LED Indicator

Connected Single Socket Outlet 16A

(See A) Reset button

(See B) Status LED

Connected Double Socket Outlet 16A

(See A) Reset button

(See B) Status LED

Smoke Alarm Battery/ Wiser Smoke Alarm 230 V/

(See A) Reset button

(See B) Standby LED

(See C) Status LED

Wiser Radiator Thermostat

(See A) Function Knob

(See B) 3 status LED

PowerTag Energy

(See A) Status LED

Connected Motion Sensor with Multiwire Dimmer

(See A) Status LED

(See B) Reset Button

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.