SUG_Wiser_Sweden_Finland_WSE-09

Dimmers

Connected Motion Sensor with Multiwire Dimmer

The Connected Motion Sensor with Multiwire Dimmer detects moving heat sources (e.g. persons) and can switch and dim ohmic, inductive or capacitive loads for a settable overtravel time.

Instruction Sheet (PDF)

Device User Guide

Connected Multiwire Universal Push-button Dimmer LED

With the Connected Multiwire Universal Push-button Dimmer LED, you can switch and dim ohmic, inductive or capacitive loads.

Instruction Sheet (PDF)

Device User Guide

Connected Multiwire Universal Rotary Dimmer LED

With the Connected Multiwire Universal Rotary Dimmer LED, you can switch and dim ohmic, inductive or capacitive loads.

Instruction Sheet (PDF)

Device User Guide

Wiser Micro Module Dimmer

Converts compatible mechanical push-button switches into smart dimmers. Connect up to 10 compatible mechanical push buttons.

NOTE: Mechanical push buttons must be certified for use in 220–240 V AC applications.

Instruction Sheet (PDF)

Device User Guide

Wiser Multiwire Micro Module LED Dimmer

TheWiser Multiwire Micro Module LED Dimmer combines the advantages of smart dimmer functionality with ordinary mechanical push-button switches.

NOTE: Mechanical push buttons must be certified for use in 220 – 240 V AC applications.

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.