SUG_Wiser_Sweden_Finland_WSE-09

Adding home members

Add members to the home so that they can operate the devices in the home using their mobile phone/tablet and the app. Home owners can also enable Administrator access for selected home members to configure and maintain the Wiser system.
NOTE: Each person to be added as a home member must have registered an app account using a country code in the same region as the home location. See Data stores and Data centre.
  1. On the home page, tap Menu icon (A), then tap Home management (B).

  2. Tap Add New Home(C) and then tap Add member (D) and enter the required details in the fields that appears in the app after tapping (D).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.