SUG_Wiser_Sweden_Finland_WSE-09

Power devices

Wiser SmartPlug 16 A

Controls various electrical devices, for example floor lamps, radios, ventilators or coffee machines, using the app. Monitor energy consumption of plugged-in devices.

Instruction Sheet (PDF)

Device User Guide

Connected Single Socket Outlet 16A - Schuko

Remotely controls and monitors the power consumption of the plugged-in load.

Instruction Sheet (PDF)

Connected double socket outlet 16A

Consists of a smart and standard outlet. The upper smart socket controls and monitors the plugged-in power. The lower standard socket provides uncontrolled and unmonitored power.

Instruction Sheet (PDF)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.