DUG_Schneider Charge_WH-04

Network settings

If the Wi-Fi® network setting has changed, update the setting in Schneider Charge via the Wiser Home app.
  1. On the Home page, tap All > Schneider Charge > Device settings.
  2. Tap Network Settings > Schneider Charge Network Setup > .
    IMPORTANT: If you have a Wiser Hub for remote monitoring and control, both the Schneider Charge and the Hub must be connected to the same Wi-Fi® network.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?