DUG_Schneider Charge_WH-04

Pairing Anti-Tripping Module with Schneider Charge

You can pair Anti-Tripping Module and Schneider Charge with each other to prevent disturbance between them.
IMPORTANT:
  • Ensure that the installation of the Anti-Tripping Module and Schneider Charge is completed as per the installation manual.

  • Do not shut down the power supply during pairing process.

Activate pairing mode

  1. Activate pairing mode in Anti-Tripping Module as mentioned below:

    1. For EVAxHPC1 module:
      Power on the module and then press COM button for 5 s to enter the pairing mode.
      All LEDs blinks green.

    2. For EVA2HPC3 module:
      Using a screw driver set the first and last DIP switch to on position and then Power on the module.
      Only System LED blinks green.

  2. Power on the Schneider Charge. When the Side indicator light turns green, press the Functional button (Push button) on Schneider Charge 3 times to activate the pairing mode.


    Side indicator light blinks blue

When both are in pairing mode, wait for a few minutes for them to connect with each other.

Upon successful pairing:

  • On EVAxHPC1 module, both Peak LED and Run LED turn solid green.

  • On EVA2HPC3 module, System LED turns green while Communication LED turn solid green.

  • On Schneider Charge, Side indicator light turns solid green.

NOTE: After successful pairing set the max. current limit in the Anti-Tripping Module, refer respective installation manual.

Unpairing / Aborting from pairing mode

Enter pairing mode as mentioned above and follow below procedure to unpair or abort pairing mode:

  • On EVAxHPC1 module: Before successful pairing, press the COM button once to abort.

  • On EVA2HPC3 modul: Before successful pairing, change the current rating using the DIP switch to abort.

  • On Schneider Charge: Press and hold the side button for 5 seconds to abort.

NOTE: It is recommended to perform the unpairing process separately for both the anti-tripping module and the charging station.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?