DUG_Schneider Charge_WH-04

Connecting/disconnecting the charger

Connecting

  1. Plug in the charging cable connector into the Schneider Charge.

  2. Plug in the charging cable connector into the electric vehicle’s inlet.

  3. The Schneider Charge’s LED indicator will change from constant green to pulsing blue.

NOTE: For information on LED color, refer to LED indication.

Disconnecting

  1. Stop charging the vehicle with Wiser Home app to unlock the charging cable from vehicle socket.

  2. Unplug the Schneider Charge’s connector from the electric vehicle’s inlet.

  3. Wind the charging cable around the Schneider Charge winding trough.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?