DUG_Schneider Charge_WH-04

Anti-Tripping Module

EVA2HPC1

EVA4HPC1

EVA2HPC3

Overview

Schneider Charge Anti-Tripping Module, when used with a Schneider Charge charging station, functions as an intelligent load management system. It continuously adjusts the charger's power output to the electric vehicle based on the available power in the home.

The load management system determines power availability by comparing the utility power limit with the home's power consumption. This consumption data is measured using a current transformer installed at the bottom of the main circuit breaker.

Communication between the Home Anti-Tripping System and the Schneider Charge charging station is established via power line communication (PLC), eliminating the need for a separate communication cable.

NOTE: The Anti-Tripping Module is specifically designed for use with Schneider Charge charging stations. Do not use it with other electrical devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?