DUG_Schneider Charge_WH-04

Tariff

Set tariff in the Wiser Home app to view energy costs and billing information.

Accurate calculation of real-time energy consumption is based on the specific contract type and tariff information. To ensure accurate cost calculations, it is important to provide the correct tariff details. This allows the system to reflect the true cost of your energy usage, helping you better understand your energy usage and manage your expenses effectively.
The cost of energy consumption is based on the contract type:

  • Flat rate

  • Peak/Off-Peak Hours rate

  • No contract

For more information on Setting Tariff, refer to the respective System User Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?