DUG_SysM - Connected Thermostat 2 A, ZB_WH-05

Pairing the device

Using the Wiser Home app, you can pair your thermostat with the Wiser Hub to access and control the thermostat.
  1. On the Home page, tap .
  2. Tap Devices > >Climate tab.
  3. Tap > Next.
    The next screen shows the thermostat joining process.
  4. Press and hold the thermostat rotary push-button (> 3 s) until Jn appears on the device.
    The wireless LED blinks amber when joining.
  5. Wait for a few seconds until the wireless LED on the thermostat turns green.
    NOTE: The wireless LED on the thermostat turns red if it is unable to connect. For more information, refer to Troubleshooting.
    Upon successful pairing, the app displays the device joining status.
  6. Assign a room to the thermostat and tap Submit.
    NOTE: If the thermostat's preset is set to P3 (Hydronic Underfloor) and it is connected to a Wiser Underfloor Heating (UFH) actuator, then assign a room and tap Next to configure UFH. Refer configuring UFH actuator to completed the setup.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?