Pairing two Dimmers
-
You can operate 2 dimmers without the need for Wireless switch as a part of Quick Home Connect.
-
One or more dimmers should be connected to a 2 gang mechanical push-button. Refer to the below wiring diagram.
-
You must put both dimmers in a pairing mode at the same time. The pairing mode will be active for about a minute.
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only
by skilled professionals. Skilled professionals must prove profound
knowledge in the following areas:
- Connecting to installation networks.
- Connecting several electrical devices.
- Laying electric cables.
- Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
HAZARD OF ELECTRIC SHOCK
- Make sure that the terminal connection area does not
come in contact with the metallic parts of any device installed in
the same location.
- Do not short the outputs to neutral.
Failure to follow these instructions will result in death or serious injury.
|
Scenario 1: Dimmer–1 is
wired to a 2 gang mechanical push-button and Dimmer–2 is
not connected to any push-button and it remotely controlled by Dimmer–1.
Upon pairing, you can control the Dimmer–2 from Dimmer–1.
-
On Dimmer–1, short press the right mechanical push button 5 times in quick succession.
-
On Dimmer–2, short press the Setup/Reset button 5 times in quick succession on the dimmer.
The light connected to the dimmer blinks for a few times. The dimmer can now be controlled by the push-button.
Operating the dimmers: Short press the push buttons to turn on/off the light as mentioned in the following table.Push button control | Load |
Left push button (Wired to terminal 1) | Light 1 |
Right push button (Wired to terminal 2) | Light 2 |
-
Press and hold the push button to adjust the brightness of the light.
NOTE: This step is same for both the (right and left) push-buttons.
Scenario 2: Both dimmers are wired
to their respective push-buttons.
Upon pairing, both
the dimmers can be controlled
vice versa. That means Dimmer–1 can
control Dimmer–2 and Dimmer–2 can
control Dimmer–1.
-
On Dimmer–2, short press the right mechanical push button 5 times in quick succession.
-
On Dimmer–1, short press the Setup/Reset button 5 times in quick succession on the dimmer.
The light connected to the dimmer blinks for a few times. The dimmer can now be controlled by the mechanical push-button.
Operating the dimmers: Short press the push buttons to turn on/off the light as mentioned in the following table.
Push button control | Load |
Dimmer 1 | |
Left push button (Wired to terminal 1) | Light 1 |
Right push button (Wired to terminal 2) | Light 2 |
Dimmer 2 | |
Left push button (Wired to terminal 1) | Light 2 |
Right push button (Wired to terminal 2) | Light 1 |
-
Press and hold the push button to adjust the brightness of the light.
NOTE: This step is same for both the (right and left) push-buttons.