DUG_Wiser jalusibrytarpuck_WH-07

Creating a moment

  1. On the Home screen, tap .
  2. Go to Moments and then tap to create a moment.
  3. Enter the name of the moment (A).
    TIP: You can choose the cover image that represents your moment by tapping .
  4. Tap Add actions (B) to select the list of devices.
  5. Select the devices (C) you want to set an action and tap Done.
  6. On the Moment creator page, select any one of the following device and set actions.
    • For shutter:
      • Drag the sliding bar up/down to open/close the shutter completely (D,E).

      • Drag the sliding bar to keep the shutter in the preferred position.

    • For Shutter slat:
      • Select Position (F) and drag the sliding bar up/down to open/close the shutter (G).

      • Select Slat Tilt (F) and drag the sliding bar up/down to adjust the tilt position of the shutter (H).

  7. Tap Set.
  8. Once all conditions are set, tap Save.
Once the moment is saved, it is visible on the Moments tab. You can tap on the moment to enable it.
FÖRSLAG:
  • If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Moments toggle switch.

  • You can also rearrange the moments by tapping Edit from the Moments tab on the Home screen, or by tapping Automation > Moments > Reorder.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Var det här till hjälp?