DUG_Wiser jalusibrytarpuck_WH-07

Pausing the seasonal comfort mode

Using the Wiser Home app, you can set the shutter position and pause the seasonal comfort mode for some time.

To pause the seasonal comfort mode:
  1. On the Control tab, select the shutter for which you want to pause the seasonal comfort mode.
    FÖRSLAG: Tap up/down button (A) to move the shutter to required position.
  2. Tap the pause button to select the time for which you want to pause the seasonal comfort mode.
    FÖRSLAG: You can tap Cancel at any time to stop the pause.
    VIKTIG: If you manually override the shutter, the system will pause for 1 hour from the time of the first manual adjustment. However, we recommend to pause the seasonal comfort mode using he Wiser Home app.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Var det här till hjälp?