DUG_ 2 Channel Dimmer Controller-00

About the device

Wiser 2 Channel Dimmer Controller is a miniature micro module (hereinafter referred to as Puck), which is remotely controlled and designed to operate in AC mains. In AC mains, it operates with a common neutral lead. Two bell switches enable ON/OFF and dimming control of regular loads. It can be used to control different types of analog/digital dimmable lights. The device also operates as a repeater within the Z-Wave network to which it is associated and uses the latest Z-Wave plus chips. Typical regular dimmer loads (2D) are: light sources and other dimmable utility appliances.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?