Configuring the device
-
Select the device from the list.
-
On the Device Control Screen, tap
.
The Device Settings screen appears.
|
A |
Device Name |
Displays the device name, tap |
|
B |
Change Room |
Displays the assigned room of the device, tap Change Room to assign any room (such as living room, bedroom, kitchen, etc.). For more information, refer to the Changing the device location topic. |
|
C |
Radio Type |
Displays the Z-Wave network. |
|
D |
Device Type |
Displays the device type. |
|
E |
Signal Strength |
Displays the signal strength. |
|
F |
Switch Type |
Allows you to change the switch type to ON/OFF Button or Push Button. |
|
G |
Advanced Settings |
Allows you to set group switches and configuration. When you tap Advanced Settings, you can see the following options:
|
|
H |
Product Details |
Displays the product details such as manufacturer name, ID, product name, ID, and type. Also you can view the firmware version and update it if a new version is available by tapping Product Details > Firmware Version & OTA. |
|
J |
Notification |
Enable the Notify Me toggle button to receive device notifications. |