DUG_ 2 Channel Dimmer Controller-00

Renaming the device

You can rename the device name using the Wiser app.

To rename the device:

  1. On the Home screen, tap Devices > Devices.
  2. Select the device for which you want to change the name.
  3. On the top-right screen, tap .
    The Device Settings screen appears.
  4. Tap and enter a new name in the name field.

    The changes will be saved automatically.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?