DUG_ 2 Channel Dimmer Controller-00

Edit favourites

You can add or remove devices and automations from the favourites list.

To remove favourites:

  1. On the Home screen, tap .
    The Edit Favourites screen appears.
  2. Tap the icon to add or remove devices and automations from the favourites list.
  3. Once complete, tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?