DUG_ 2 Channel Dimmer Controller-00

Resetting the device

You can reset the device to factory default manually.

For resetting the micro module:

  1. Press and hold the Programming button for <10 s.
  2. After 10 s, LED starts blinking red then release the programming button.
    NOTE: All configuration data, user data, and network data are deleted. After which
    • No connectivity to other devices or rooms.

    • No moment or schedule settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?