DUG_ 2 Channel Dimmer Controller-00

Adjusting the brightness level using app

Using the Wiser app, you can increase or decrease the brightness level of the dimmer.
  1. On the Home screen, tap Devices > Devices.
  2. Select the dimmer.
  3. On the Device Control Screen, drag the sliding bar (A) left/right to increase/decrease the brightness.
    TIP: You can also tap (B) to turn ON/OFF the dimmer.
    NOTE: Some lamps have a starting point. When you turn on the lamp at a low brightness, it quickly gets very bright and then automatically returns to the lower brightness. This is the behavior of the lamp, and the dimmer can't change it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?