DUG_ 2 Channel Dimmer Controller-00

Manual operation

When the puck is connected to a bell switch, the connected lighting devices can be controlled manually.

  • Short press the bell switch to turn ON/OFF the light.

  • Press and hold the bell switch to adjust the dimming level of the light.

NOTE: When the puck is installed inside the wall box, the status LED is not visible while using the puck.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?