DUG_ 2 Channel Dimmer Controller-00

Turning ON/OFF dimmer using app

Using the Wiser app, you can turn ON/OFF the dimmer.

Turn the device ON/OFF:

  1. On the Home screen, tap Devices > Devices.
  2. Find the device you want to turn ON/OFF.
  3. Tap (A) to turn ON/OFF the dimmer.
    TIP:
    • You can also turn the device ON/OFF from the Device Control Screen.

    • Additionally, turn the device ON/OFF when you add it to your Favourites. To know more about Favourites, refer to the Add Favourites topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?