DUG_ 2 Channel Dimmer Controller-00

Removing the device

Using the Wiser app, you can remove a device from the device list.

To remove a device:

  1. On the Home screen, tap Devices > Devices.
  2. On the top-right pane, tap .
    The Edit Devices screen appears.
  3. Tap on the device that you want to remove from the Wiser system.
    The Delete message pop-up appears.
  4. Tap Confirm.
    Wait for a few seconds, and the successful message appears on the screen.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to .
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?