SUG_Wiser_India-00

Creating a user account

To control the devices from your smartphone, you need to create an account and log in.
  1. To create a user account, tap onSettings and then select User Management.
  2. Click on + to add a new user.
  3. Enter all mandatory fields (Username, password, time, authority etc).
    NOTE: The users can be assigned different authorities:
    • The ‘Scene’ authority will allow user to use the scenes/shortcut functions only.

    • The ‘Control’ authority will allow the user to control everything but no modifications.

    • The Settings’ authority will allow user to do any task as well as modifications, except the user management.

    • Click on Update to save the changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?