SUG_Wiser_India-00

Setting up the Wiser Automation Gateway with Ethernet

The app allows you to setting up a Wiser System with Ethernet and add devices to the Wiser Automation Gateway.
Before setting up the Wiser Automation Gateway with Internet router, connect the Ethernet cable to the Wiser Automation Gateway. Also, connect your mobile device to the Wi-Fi network.

To set up the Wiser System:
  1. Power up the Wiser Automation gateway using the adapter.
  2. Connect the gateway to the internet router using an Ethernet (LAN) cable.
  3. Wait until the red and blue lights on the gateway appears solid.
  4. Log in to the Wiser India app on your mobile device.
  5. Select Add Gateway / Smart doorbell
  6. On the Setup page, tap Setup (A) and select the Gateway IH101ZWIFI and tap on Connect (B).
  7. On the Device page, tap Devices.
  8. Tap + > All > B.One Edge 3.0.
    The IH101ZWIFI Gateway Setup page appears.
  9. On the Setup page, add the following Wiser Automation gateway information:
    • Name (C): Add the device name.

    • Enter Device ID or Scan QRCode (D): You can find the these information on the back side of the Gateway.

    • Gateway Username (E): Add the name as per your requirement.

    • Gateway Password (F): provide password as per your requirement.

    • Tap on Setup (G) to finish the setup.

    Wait for a few minutes, and you will see the Gateway info screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?