SUG_Wiser_India-00

Editing a moment

  1. On theMomentspage, locate the moment you want to edit.
  2. Slide left on the selected moment, it will show the option to edit and delete, tap EDIT.
  3. On the EDIT page, you can tap each item (Such as Dimmer, Fan, 4 channel relay, Curtain controller, etc.) to change the settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?