SUG_Wiser_India-00

Selecting the Mounting Location

The ideal location for the Wiser Automation Gateway is determined by the following:

  • Layout of the building where the system is installed

  • Location of other devices that will be used in the system

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?