SUG_Wiser_India-00

Removing the device

Using the Wiser India app, you can remove a device from the device list.


To remove the device:
  1. On the Home page, tap Device.
  2. Tap Remove > Other Z-Wave device > YES (If you heard the beep sound).
    NOTE:
    • Removing the device will reset the Puck. After reset, the LED turns RED indicating that the Puck is ready to pair with another network.

    • For more information, please refer to the video: How to remove the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?