Limitations of the Wiser System
System Limits
| Maximum number of | Supported/Not Supported | Remarks |
|---|---|---|
|
Z-Wave devices |
120 |
We practically verified with 50-60 devices (Around 30+ power based and remaining sleepy/battery based devices). |
|
Moment and Schedule |
Supported |
We verified maximum 60 actions can created. |
|
Multiple Automation Gateway compatible |
Supported |
|
|
Can we add any Brand and any type of Z-Wave device? |
No H/W is supported |
Devices which are not part of the Mobile App, Need customization in the Firmware based on the device type and the features supported. Some devices get added but may not function properly. |
|
What is the range of the Z-Wave devices can be connected ? (Ex - 2000 sqft home ) |
It depends on the constructed area and Z-Wave network formation. |
|
|
Max. no. of devices in one Location (Z-Wave) |
Verified |
60 devices |
|
Max. no. of devices in one Room (Z-Wave) |
Not verified |