SUG_Wiser_India-00

Setting up the Wiser Automation Gateway

In order to be able to control the system via your smartphone, the Wiser Automation Gateway must be connected to the internet.

You can set up the Wiser Automation Gateway by using the Ethernet:

  1. Use the adapter provided in the box to power up the Wiser Automation Gateway.

  2. Connect the Wiser Automation Gateway to the internet router using a LAN Cable.

  3. Wait until the gateway displays solid red and blue lights.

You can set up the Wiser Automation Gateway by using the Wiser India app. Refer to

You can setup the Wiser System by using the app after creating an account. Refer to for information on how to create an account.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?