SUG_Wiser_India-00

Decommissioning a Wiser System

To remove a device from your Home or prepare the Home for a new user, follow these steps:

  • Remove all devices from the system.

  • Reset all devices to the factory settings.

  • Reset the Wiser Automation Gateway to the factory settings.

Removing a device

Possible reasons:

  • The device needs to be replaced.

  • The device is no longer needed in the Wiser System.

Steps:

  • Remove the device from the Wiser System. Refer to Removing the device.

  • Reset the device to the factory settings.

    Find the details of resetting the device in the Device User Guide of the respective device: List of Wiser Devices

Resetting the Wiser System

Possible reasons:

  • You are moving out of the house and want to prepare it for the next owner.

  • Ownership of the Wiser System is to be transferred to another user.

Steps:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?