SUG_Wiser_India-00

Resetting the Wiser Automation Gateway Manually

You can reset the Wiser Automation Gateway to its factory defaults.

NOTE: Resetting the Wiser Automation gateway will delete the Wiser System you have set up. If you want to reinstall your System, you will have to also reset all your connected devices and add them again to your system. Refer to resetting the device chapter in the Device User Guide of the respective device. List of Wiser Devices provides the links to Device User Guide for each devices. You will have to recreate all schedules, moments, automations, etc.

Only use the reset when you want to decommission your Wiser System or if all other troubleshooting measures failed.

To reset the Wiser Hub to factory defaults:

  1. Press and hold the Reset button until the LED turns solid Blue.

This indicates that the Wiser Automation Gateway is successfully reset.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?