Add ArcFM SOE to ArcGIS Server

Wavepoint is enabled after you add its Server Object Extension (SOE) to the ArcGIS Server Manager.

  1. Navigate to ArcGIS Server Manager, and log in with your server credentials.

  2. Click Site at the top of the page.
  3. Click Extensions from the menu on the left.
  4. Click Add Extension.

  5. Click Choose File and navigate to the ArcGIS Server installation directory's bin folder, i.e., ...\Program Files\ArcGIS\Server\bin.
  6. Select Miner.Server.soe and click Open.

  7. Click Add.
  8. Verify you see the extension when complete.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.