Create the Source Map for the Published Service

The Wavepoint map with your fiber assets and other reference feature classes starts as an .mxd (or Stored Display) in ArcMap. The following help topics discuss requirements and recommendations for this source map.

TIP: If you already have a Stored Display with your fiber assets, that is a great starting point, but still read through the entirety of these topics to ensure your existing Stored Display is ready to publish as a service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.