Wavepoint Configuration Overview

Before You Begin

Ensure the computer you are using as the server has adequate hardware for the task. Only 64-bit environments are supported. You must have valid licenses to configure and run Wavepoint.

IMPORTANT: Visit the myArcFM page Wavepoint - Supported Versions for the most up-to-date information about supported versions.

Choose Hardware Structure

There are four components to Wavepoint:

  • The geodatabase, which is the source of data for a published web service

  • ArcMap/ArcFM to manage the underlying data and publish the web service

  • ArcGIS server to manage access to the service once published

  • The Wavepoint web application

You can choose between two supported hardware structures to host each of these four components:

  • On a single machine

  • Separately on multiple machines

Client Machines Requirements

The client machines must run one of the following supported web browsers:

  • Google Chrome

  • Mozilla Firefox

  • Internet Explorer 9 and above

    IMPORTANT: Active Scripting must be enabled in Internet Explorer.

Supported Versions

Information about supported versions and required licenses is updated on myArcFM.

IMPORTANT: Visit the myArcFM page Wavepoint - Supported Versions for the most up-to-date information about supported versions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.